Typical PowerAlert Configurations
Desktop Workstation or Single Server
Multiple Computers Attached to a Single UPS

Small Network Configurations
Multiple Computers Attached to a Single UPS

Server With Redundant Power Supplies

Small-to-Medium Network Configurations
Computer(s) Connected to UPS via Local Area Network

Use this configuration when it is not possible for the UPS or PDU to connect to the computer(s) via a USB or serial communication port. An SNMP Network Card (SNMPWEBCARD) must be installed in the UPS or PDU. An SNMP Network Card also supports device monitoring and control over the Internet via a browser.
Medium-to-Large Network Configurations
Computer(s) Connected to UPS via Local Area Network

To monitor and control a UPS or PDU over the Internet via a browser, the device must have an SNMP Network Card (SNMPWEBCARD) installed.